Difference between LPC1124 and LPC1125

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Difference between LPC1124 and LPC1125

2,260 次查看
dhananjay_patil
Contributor I

Hello NXP Team,

What are differences between LPC1124 and LPC1125 except flash size?

Are they pin to pin compatible?

Regards,

Dhananjay Patil 

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

2,207 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Dhananjay Patil 

Yes, besides Flash, there is no difference. these two parts are pin to pin compatible.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复