Difference between LPC1124 and LPC1125

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Difference between LPC1124 and LPC1125

2,224件の閲覧回数
dhananjay_patil
Contributor I

Hello NXP Team,

What are differences between LPC1124 and LPC1125 except flash size?

Are they pin to pin compatible?

Regards,

Dhananjay Patil 

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

2,171件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Dhananjay Patil 

Yes, besides Flash, there is no difference. these two parts are pin to pin compatible.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信