Deep power down on LPC1517

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Deep power down on LPC1517

Jump to solution
3,303 Views
martin_pelletie
Contributor II

I try to use the deep power down. 

i use this code on xxx.h:

#define DEEP_POWER_DOWN 3
typedef struct PWRD_API {
void (*set_pll)(uint32_t cmd[], uint32_t resp[]); /*!< Set PLL function */
void (*set_power)(uint32_t cmd[], uint32_t resp[]); /*!< Set power function */
/*!< Sets the chip in low power modes */
void (*power_mode_configure)(unsigned int mode, unsigned int peripheral);
void (*reserved1)();
void (*reserved2)();
} PWRD_API_T;
typedef struct _ROM {
const PWRD_API_T * pPWRD;
} ROM;

#define ROM_DRIVER_BASE (0x03000200UL)
#define LPC_PWRD_API ((PWRD_API_T *) ((*(ROM * *) (ROM_DRIVER_BASE))->pPWRD))

and this code on file.c: to put on deep power down

if (analogValueLen > 0xC00)
{
//deep power down
LPC_PWRD_API->power_mode_configure(DEEP_POWER_DOWN,0);
__WFI();
}

main.c file:

int main (void) 

{

//GPIO init

LPC_SYSCON->SYSAHBCLKCTRL0 |= (1UL << 13); /* enable clock for IOCON0 */
LPC_SYSCON->SYSAHBCLKCTRL0 |= (1UL << 14); /* enable clock for GPIO0 */
LPC_SYSCON->SYSAHBCLKCTRL0 |= (1UL << 15); /* enable clock for GPIO1 */
LPC_SYSCON->SYSAHBCLKCTRL0 |= (1UL << 16); /* enable clock for GPIO2 */

LPC_GPIO_PORT->DIR[0] = 0; //input

...

if (LPC_PMU->PCON & 0x00800) //bit 11
{
LPC_PMU->PCON |= 0x00800; //reset le flag!!!!
PDownDetected = 1;
}
else
PDownDetected = 0;

...

}

My question is : i cant wake up the deep power down!!!

The wake up pin (pin #28) has a pullup resistor and if i send a ground pulse or a ground level, it is supposed to wake up the lpc1517 by the POR and the chip re-boots!!!! But nothing happens!!! Am i missing something!!!!

thx in advance for your help!!!!

Labels (1)
1 Solution
2,968 Views
martin_pelletie
Contributor II

Thx Victor for your helps :smileyhappy:

I found my problem (pointer location!!!) and i want to post it!!

In my file calcul.h, i have this code:

#define SLEEP 0
#define DEEP_SLEEP 1
#define POWER_DOWN 2
#define DEEP_POWER_DOWN 3

typedef struct PWRD_API {
void (*set_pll)(uint32_t cmd[], uint32_t resp[]); /*!< Set PLL function */
void (*set_power)(uint32_t cmd[], uint32_t resp[]); /*!< Set power function */
void (*power_mode_configure)(unsigned int mode, unsigned int peripheral);
void (*reserved1)();
void (*reserved2)();
} PWRD_API_T;

typedef struct _ROM {
const unsigned p_dev0;
const unsigned p_dev1;
const unsigned p_dev2;
const PWRD_API_T * pPWRD; /* ROM Power Management API */
const unsigned p_dev4;
const unsigned p_dev5;
const unsigned p_dev6;
const unsigned p_dev7;
} ROM_API;

and on my main.c

#include "calcul.h"

...

static ROM_API ** romAPI = (ROM_API **) 0x03000200; /* pointer to power API calls */

...

int main(void)

{

  ...

  if (LPC_PMU->GPREG0 == 1) //came from deep power down
      PDownDetected = 1;
  LPC_PMU->PCON |= 0x00100; //PMU_PCON_SLEEPFLAG->reset le flag!!!!
  LPC_PMU->PCON |= 0x00800; //PMU_PCON_DPDFLAG->reset le flag!!!!
  LPC_PMU->DPDCTRL = 1; //enable hysterisis
  LPC_PMU->DPDCTRL &= ~(1UL << 1); //Wake-up function is enable on pin PIO0_17

  ...

  if (GPIO_ReadPin(IN_PWD_STATUS) == 0)  //0 = normal mode  and 1 means power down

  {

  ...

  }

  else

  {

     (*romAPI)->pPWRD->power_mode_configure(3, 0); //DEEP_POWER_DOWN
     __WFI();

  }

}

View solution in original post

3 Replies
2,969 Views
martin_pelletie
Contributor II

Thx Victor for your helps :smileyhappy:

I found my problem (pointer location!!!) and i want to post it!!

In my file calcul.h, i have this code:

#define SLEEP 0
#define DEEP_SLEEP 1
#define POWER_DOWN 2
#define DEEP_POWER_DOWN 3

typedef struct PWRD_API {
void (*set_pll)(uint32_t cmd[], uint32_t resp[]); /*!< Set PLL function */
void (*set_power)(uint32_t cmd[], uint32_t resp[]); /*!< Set power function */
void (*power_mode_configure)(unsigned int mode, unsigned int peripheral);
void (*reserved1)();
void (*reserved2)();
} PWRD_API_T;

typedef struct _ROM {
const unsigned p_dev0;
const unsigned p_dev1;
const unsigned p_dev2;
const PWRD_API_T * pPWRD; /* ROM Power Management API */
const unsigned p_dev4;
const unsigned p_dev5;
const unsigned p_dev6;
const unsigned p_dev7;
} ROM_API;

and on my main.c

#include "calcul.h"

...

static ROM_API ** romAPI = (ROM_API **) 0x03000200; /* pointer to power API calls */

...

int main(void)

{

  ...

  if (LPC_PMU->GPREG0 == 1) //came from deep power down
      PDownDetected = 1;
  LPC_PMU->PCON |= 0x00100; //PMU_PCON_SLEEPFLAG->reset le flag!!!!
  LPC_PMU->PCON |= 0x00800; //PMU_PCON_DPDFLAG->reset le flag!!!!
  LPC_PMU->DPDCTRL = 1; //enable hysterisis
  LPC_PMU->DPDCTRL &= ~(1UL << 1); //Wake-up function is enable on pin PIO0_17

  ...

  if (GPIO_ReadPin(IN_PWD_STATUS) == 0)  //0 = normal mode  and 1 means power down

  {

  ...

  }

  else

  {

     (*romAPI)->pPWRD->power_mode_configure(3, 0); //DEEP_POWER_DOWN
     __WFI();

  }

}

2,968 Views
martin_pelletie
Contributor II

It seems like the external pin PIO0_17 (WAKEUP pin)  is not worked!!!!!

If i put a gnd on it, the lpc stays all the time in deep power down!!!

thx for your helps!!!

0 Kudos
Reply
2,968 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Martin,

I took as an example the project periph_pmu of the LPCOpen v2_20 for the LPC1549. I modified this project in order to wake up the LPC with the pin PIO0_17 and I didn't face any problems, here is the main of my project.

int main(void)
{
     /* Setup SystemCoreClock and any needed board code */
     SystemCoreClockUpdate();
     Board_Init();
     Board_LED_Set(0, true);

     /* Clear any previously set deep power down and sleep flags */
     Chip_PMU_ClearSleepFlags(LPC_PMU, PMU_PCON_SLEEPFLAG | PMU_PCON_DPDFLAG);

     DEBUGSTR("\r\n");
     DEBUGSTR("-----------------------------------------------------------------\r\n");
     DEBUGOUT("Power Control Example   Cycle Count: \r\n");
     DEBUGSTR("  System will go to DEEP POWER DOWN power state\r\n");
     DEBUGSTR("  press SW1 to exit\r\n");
     DEBUGSTR("-----------------------------------------------------------------\r\n\r\n");

     if(0 == LPC_PMU->GPREG[0])
     {
          DEBUGSTR("-----------------------------------------------------------------\r\n");
          DEBUGSTR("     Entering DEEP POWER DOWN power setting\r\n");
          DEBUGOUT("       (System will exit DEEP POWER DOWN by pressing SW1)\r\n");
          DEBUGSTR("-----------------------------------------------------------------\r\n\r\n");
          LPC_PMU->GPREG[0] = 1;
          delay();
          Chip_PMU_DeepPowerDownState(LPC_PMU);
     }
     else
     {
          DEBUGSTR("-----------------------------------------------------------------\r\n");
          DEBUGSTR("     System WAKE UP\r\n");
          DEBUGOUT("       Led will start to Toggle\r\n");
          DEBUGSTR("-----------------------------------------------------------------\r\n\r\n");
     }

     while (1)
     {
          Board_LED_Toggle(0);
          delay();
     }

     return 0;
}‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

 Also, I recommend you checking sections 4.4, 4.7.6, 4.7.6.2 and 4.7.6.3 of the user manual.

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply