Debugging getting failed with incorrect request of memory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debugging getting failed with incorrect request of memory

2,782 Views
VishnuBoyapati
Contributor I

I am facing the bellow errors when trying to debug on LPCxpresso55s69 board and am unsure why these memory locations are getting accessed. I see the executable is being written on the flash succesfully but going into these errors. I referred to "Edit MCU" done wrong results in "Wire ACK Fault i... - NXP Community which is the same issue as this, but the solution isn't working. I am attaching the MCU memory layout.

 

Flash Write Done
Flash Program Summary: 14372 bytes in 0.05 seconds (275.20 KB/sec)
Starting execution using system reset and halt target with a stall address
Retask read watchpoint 1 at 0x50000040 to use for boot ROM stall
Boot ROM stalled accessing address 0x50000040 (restoring watchpoint 1)
Stopped (Was Reset) [Reset from Unknown]

 

Labels (1)
0 Kudos
Reply
1 Reply

2,765 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

Which version of MCUXpresso IDE you used? 

Please try MCUXpresso IDE v11.5.

 

BR

Alice

0 Kudos
Reply