Debugging EMC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugging EMC

1,144件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by arainho on Tue Jan 29 03:21:02 MST 2013
HI All,

I am debugging a new board and I am having a bit of trouble with EMC (with a MT48LC4M32B2P).

It's basicaly working but when I write to one memory address say 0xa0000 0000 it´s replicated at 0xa0000 0100, it I write at 0xa0000 0100 it also writes at 0xa0000 0000. So basicaly 256 bytes replicate to the next 256 bytes. I tought it might be a short in the address lines, but have checked all address lines and they are ok. It also does the same thing when I change to Row, Bank, Col mode.

Any ideas on debugging this.

Thanks,

Alfredo

===================================================

void EMCInit(void)
{
  volatile uint32_t CmdDly;
  volatile uint32_t Dummy;
  volatile uint32_t i;

  LPC_SC->PCONP     |= (1 << 11);   // Turn on EMC peripheral clock
  LPC_SC->EMCDLYCTL  = 0x00001010;
  LPC_EMC->Control   = 1;           // EMC enable
  LPC_EMC->Config    = 0;
  //
  // Port init
  //
  LPC_IOCON->P3_0  |= 1;  // D0
  LPC_IOCON->P3_1  |= 1;  // D1
  LPC_IOCON->P3_2  |= 1;  // D2
  LPC_IOCON->P3_3  |= 1;  // D3
  LPC_IOCON->P3_4  |= 1;  // D4
  LPC_IOCON->P3_5  |= 1;  // D5
  LPC_IOCON->P3_6  |= 1;  // D6
  LPC_IOCON->P3_7  |= 1;  // D7
  LPC_IOCON->P3_8  |= 1;  // D8
  LPC_IOCON->P3_9  |= 1;  // D9
  LPC_IOCON->P3_10 |= 1;  // D10
  LPC_IOCON->P3_11 |= 1;  // D11
  LPC_IOCON->P3_12 |= 1;  // D12
  LPC_IOCON->P3_13 |= 1;  // D13
  LPC_IOCON->P3_14 |= 1;  // D14
  LPC_IOCON->P3_15 |= 1;  // D15
  LPC_IOCON->P3_16 |= 1;  // D16
  LPC_IOCON->P3_17 |= 1;  // D17
  LPC_IOCON->P3_18 |= 1;  // D18
  LPC_IOCON->P3_19 |= 1;  // D19
  LPC_IOCON->P3_20 |= 1;  // D20
  LPC_IOCON->P3_21 |= 1;  // D21
  LPC_IOCON->P3_22 |= 1;  // D22
  LPC_IOCON->P3_23 |= 1;  // D23
  LPC_IOCON->P3_24 |= 1;  // D24
  LPC_IOCON->P3_25 |= 1;  // D25
  LPC_IOCON->P3_26 |= 1;  // D26
  LPC_IOCON->P3_27 |= 1;  // D27
  LPC_IOCON->P3_28 |= 1;  // D28
  LPC_IOCON->P3_29 |= 1;  // D29
  LPC_IOCON->P3_30 |= 1;  // D30
  LPC_IOCON->P3_31 |= 1;  // D31

  LPC_IOCON->P4_0  |= 1;  // A0
  LPC_IOCON->P4_1  |= 1;  // A1
  LPC_IOCON->P4_2  |= 1;  // A2
  LPC_IOCON->P4_3  |= 1;  // A3
  LPC_IOCON->P4_4  |= 1;  // A4
  LPC_IOCON->P4_5  |= 1;  // A5
  LPC_IOCON->P4_6  |= 1;  // A6
  LPC_IOCON->P4_7  |= 1;  // A7
  LPC_IOCON->P4_8  |= 1;  // A8
  LPC_IOCON->P4_9  |= 1;  // A9
  LPC_IOCON->P4_10 |= 1;  // A10
  LPC_IOCON->P4_11 |= 1;  // A11
  LPC_IOCON->P4_12 |= 1;  // A12
  LPC_IOCON->P4_13 |= 1;  // A13
  LPC_IOCON->P4_14 |= 1;  // A14
 
  LPC_IOCON->P4_25 |= 1;  // WE
  LPC_IOCON->P2_16 |= 1;  // CAS
  LPC_IOCON->P2_17 |= 1;  // RAS
  LPC_IOCON->P2_28 |= 1;  // DQMOUT0
  LPC_IOCON->P2_29 |= 1;  // DQMOUT1
  LPC_IOCON->P2_30 |= 1;  // DQMOUT2
  LPC_IOCON->P2_31 |= 1;  // DQMOUT3
  LPC_IOCON->P2_18 |= 1;  // CLKOUT0
  LPC_IOCON->P2_19 |= 1;  // CLKOUT1
  LPC_IOCON->P2_24 |= 1;  // CKEOUT0
  LPC_IOCON->P2_20 |= 1;  // DYCS0

  //
  // Setup EMC config for SDRAM, timings for 60MHz bus
  //
  LPC_EMC->DynamicConfig0    = 0x00005500;  // 128MB, 4Mx32, 4 banks, 12 rows, 8 columns, buffers disabled
  LPC_EMC->DynamicRasCas0    = 0x00000202;  // 2 RAS, 2 CAS latency */
  LPC_EMC->DynamicReadConfig = 0x00000001;  // Command delayed strategy, using EMCCLKDELAY
  LPC_EMC->DynamicRP         = 0x00000002;  // n + 1 clock cycles
  LPC_EMC->DynamicRAS        = 0x00000005;  // n + 1 clock cycles
  LPC_EMC->DynamicSREX       = 0x00000008;  // n + 1 clock cycles
  LPC_EMC->DynamicAPR        = 0x00000001;  // n + 1 clock cycles
  LPC_EMC->DynamicDAL        = 0x00000005;  // n     clock cycles
  LPC_EMC->DynamicWR         = 0x00000001;  // n + 1 clock cycles
  LPC_EMC->DynamicRC         = 0x00000008;  // n + 1 clock cycles
  LPC_EMC->DynamicRFC        = 0x00000008;  // n + 1 clock cycles
  LPC_EMC->DynamicXSR        = 0x00000008;  // n + 1 clock cycles
  LPC_EMC->DynamicRRD        = 0x00000001;  // n + 1 clock cycles
  LPC_EMC->DynamicMRD        = 0x00000001;  // n + 1 clock cycles
  delayMs(100);
  LPC_EMC->DynamicControl    = 0x00000183;  // Issue NOP command
  delayMs(200);
  LPC_EMC->DynamicControl    = 0x00000103;  // Issue PALL command
  LPC_EMC->DynamicRefresh    = 0x00000002;  // n * 16 clock cycles
  for (i = 0; i < 0x80; i++);               // Wait 128 AHB clock cycles
  LPC_EMC->DynamicRefresh    = 0x0000003A;  // n * 16 clock cycles
  //
  // Init SDRAM
  //
  LPC_EMC->DynamicControl = 0x00000083;                             // Issue MODE command
  Dummy = *((volatile uint32_t*)(SDRAM_BASE_ADDR | (0x22 << (8+2))));  // 4 burst, 2 CAS latency , col row bank
  LPC_EMC->DynamicControl = 0x00000000;                             // Issue NORMAL command
  LPC_EMC->DynamicConfig0 = 0x000085500;                            // Enable buffers
  //
  // Auto calibrate timings
  //
  CmdDly = _CalibrateOsc();
  //
  // Find best delay values
  //
  _TestSDRAM();

  _FindDelay(0);  // EMCDLY
  _FindDelay(1);  // FBCLKDLY
  _AdjustEMCTiming(CmdDly);
}
ラベル(1)
0 件の賞賛
返信
1 返信

1,038件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by arainho on Tue Jan 29 12:05:31 MST 2013
Hi

Decided to replace the SDRam chip and now it´s working like it should!

Alfredo
0 件の賞賛
返信