Debugger and Dev Tools

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debugger and Dev Tools

1,467 次查看
bforeman
Contributor I

I just ordered the position/orientation sensor dev kit LPC54102. It comes with some sort of Windows app but I expect I will want to create my own firmware for it. What is the recommended (best supported) ARM IDE for this board and which Segger debugger box has the right functions and pinout for download to this board? As for the IDE, the best would be the one that NXP Support likes to use so I could package up a project and send it to them in case I need support.

0 项奖励
回复
1 回复

1,403 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Bret Foreman o

NXP has MCUXpresso IDE which is free of charge

MCUXpresso IDE|Eclipse-based Integrated Development Environment (IDE) | NXP 

and SDK package:

MCUXpresso SDK | Software Development for Kinetis, LPC, and i.MX MCUs | NXP 

Besides, Keil and IAR also has IDE can support LPC product.

MCUXpresso SDK can also support Keil MDK and IAR.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复