DTLS server based on mbedTLS LPCXpresso55S16

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DTLS server based on mbedTLS LPCXpresso55S16

1,603件の閲覧回数
ahmed007
Contributor II

I want to create a DTLS server using the mbedTLS library for the LPCXpresso55s16. Does anyone have a tutorial to follow?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,592件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel and I will be supporting your case, could you elaborate further on your question? I mean this is the board you mentioned but the EVK and the SDK do not have examples with LWIP. LPCXpresso55S16 Development Board | NXP Semiconductors

Best regards,
Pavel

0 件の賞賛
返信

1,574件の閲覧回数
ahmed007
Contributor II

Hello Pavel,

Thank you for your support. I am currently using SDK_2.13.0_LPCXpresso55S16, which includes the following middleware: USB Type-C PD Stack, USB Host, Device, OTG Stack, PKCS #11, mbedTLS, and CANopen. My goal is to create a DTLS server on the LPCXpresso board to enable communication with a Raspberry Pi for testing a certificate management system. The communication between the devices will be via CANopen FD. If you have any ideas or suggestions on how I can configure the LPCXpresso board as the DTLS server and establish communication via CANopen, I would greatly appreciate your input.

Thank you.

0 件の賞賛
返信

1,562件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, here is the SDK with all the examples maybe this could help you to achieve what you want to do, but I do not know an example that completely does that, I mean you may need to combine many examples.

Select Board | MCUXpresso SDK Builder (nxp.com)

Best regards,
Pavel

0 件の賞賛
返信