DFU supported with LPC1857 And IAP Command Code 57 (Reinvoke ISP)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DFU supported with LPC1857 And IAP Command Code 57 (Reinvoke ISP)?

971件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shansohn on Wed Dec 12 14:29:06 MST 2012
I have an LPC1857 device that only supports firmware upgrade via USB0/DFU (hardwired per Table 13 of UM10430).

I'd like the application code to reinvoke ISP USB0/DFU on user command to upgrade firmware.

Q1: Can the Reinvoke ISP (IAP code 57) be used for this, or will that only support ISP via UART0?

Q2: If not, how would I reset the device so it enumerates back as a DFU-mode device. (e.g. invalidate the currently running flash bank so that ISP USB0/DFU mode will be run on the next device reset?)
ラベル(1)
0 件の賞賛
返信
0 返答(返信)