DALI LPC1114 Slave BOM Detailed Description

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DALI LPC1114 Slave BOM Detailed Description

2,415件の閲覧回数
yribeiro
Contributor I

Hi,

I'm trying to assembly the DALI Slave LPC1114 and I do need some help with the Bill of Materials (BOM). Does anyone can give a detailed description of the following BOM elements?

PartValueDevicePackageDescription                                                                Remarks
D1LED0805LEDCHIPLED_0805CHIPLED_0805LED
Q212MHzCRYSTAL4XTAL4 
U$1FIDUCIAL_0.6-1.2MM FIDUCIAL_0.6-1.2MMFIDUCIAL0.6-1.2 
U$2FIDUCIAL_0.6-1.2MM FIDUCIAL_0.6-1.2MMFIDUCIAL0.6-1.2 
X4 MA14-1WMA14-1WPIN HEADER

Can I use any LED and any 12 Mhz Crystal? What FIDUCIAL_0.6 means? Does  the PIN Header have some specification?

Regards,

Yuri.

ラベル(1)
タグ(3)
3 返答(返信)

2,293件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Yuri,

The D1 is a LED with 0805 package, you can use any LED, which only indicates that the LPC1113 works fine by toggling constantly. The Q2 is a 12MHz crystal with 4 pins, you can use any crystal with 12MHz.

Regarding the FIDUCIAL_0.6 , I do not know. I will ask the other engineers for help.

BR

Xiangjun Rong

2,293件の閲覧回数
yribeiro
Contributor I

Hi, Xiangjun Rong,
Thank you for helping me! I'm waiting anxiously for the other comming answers.
Best regards,

Yuri.

0 件の賞賛
返信

2,293件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Yuri,

Maybe this link is helpful to understand the spec FIDUCIAL, which I get from Google.

http://www.pcb-3d.com/tutorials/what-is-a-fiducial-mark/ 

BR

XiangJun Rong

0 件の賞賛
返信