Need help with most basic configuration LPC804.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need help with most basic configuration LPC804.

1,926 Views
pmchoudek
Contributor I

Hello,

I am using the LPC804M101DJH24 package for my project.  I have it mounted on a 24-DIP so I can plug it into my breadboard.  I am trying to program it with Arm Keil and using the ST-Link V2 STM8 & STM32 USB debugger.  I have tried to run example code I downloaded from NXP but to no avail.  It builds without any problem, but when I go into the debugger mode it will never reach the main() function.  It seems to get stuck in the startup/boot process.

I have the same problem when I try to run my own code.  I have the proper header files I believe (LPC804.h) but it still won't run to the main() when I try to debug.  Therefore I don't think it is actually executing any code.  In the example code from NXP, the header file is (LPC8xx.h) and I think it may not be targeting my chip correctly.  I think this because of the notes at the top of the (keil_startup.s) file.

I am asking here because I want help with literally the most basic configuration I need to get my chip working.  I just want something to work on my chip because I have been stuck like this for a while.  GPIO would be something simple I can start with.

How I have the debugger connected to the chip:

I have 3.3V going to VDD pin

I have GND going to VSS pin

I have RST going to reset pin and also have a pull-up resistor to 3.3V

I have SWDIO going to SWDIO pin and also have a pull-up resistor to 3.3V

I have SWCLK going to SWCLK pin and also have a pull-down resistor going to ground.

These are the SWD connections recommended in the NXP LPC804 User manual (UM11065).

I will attach the code I have been trying to get working.  Please help me.

Thank you,

Peter

Tags (2)
0 Kudos
Reply
1 Reply

1,782 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Peter Choudek,

    I am don't know whether your ST-LINK can support the NXP LPC product or not, maybe it can't support it.

    We suggest you to use our LPC-LINK2 tool, the link is:

    LPC-Link2 | NXP 

  This tool can be CMSIS DAP or the JLINK debugger.

   I think you can use the JLINK commander to connect your board, whether you can find the ARM core or not?

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply