Current issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Current issue

1,373件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by prabhakaran on Thu Jul 03 22:31:34 MST 2014
I am using lpc1227. In that i want  to know the minimum and maximum current consumption. Because before programming it consumes 30mA and after programming Mother board consumes 70mA. so i want to reduce current . Please give suggestion the ways for current reduction.
ラベル(1)
0 件の賞賛
返信
1 返信

1,318件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxp_apps on Sat Jul 26 14:29:30 MST 2014
Hi,

We don't have maximum power consumption for the lpc122x.
But to lower power consumption and understand the low power mode options, please refer to the application note below:

http://www.lpcware.com/content/nxpfile/an11069-lpc122x-power-modes-v10

Hope this helps.

Thanks.

nxp_support
0 件の賞賛
返信