Current issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Current issue

1,469 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by prabhakaran on Thu Jul 03 22:31:34 MST 2014
I am using lpc1227. In that i want  to know the minimum and maximum current consumption. Because before programming it consumes 30mA and after programming Mother board consumes 70mA. so i want to reduce current . Please give suggestion the ways for current reduction.
Labels (1)
0 Kudos
Reply
1 Reply

1,414 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxp_apps on Sat Jul 26 14:29:30 MST 2014
Hi,

We don't have maximum power consumption for the lpc122x.
But to lower power consumption and understand the low power mode options, please refer to the application note below:

http://www.lpcware.com/content/nxpfile/an11069-lpc122x-power-modes-v10

Hope this helps.

Thanks.

nxp_support
0 Kudos
Reply