Convert to grayscale

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Convert to grayscale

1,169件の閲覧回数
thomasjohansen
Contributor I

Hi

 

I'm using the LPC1788 with a 16 bpp Color TFT display.

Is it somehow possible to get the LCD controller to convert the colors to gray scale?

 

Or do I need to convert the colors elsewhere. GUI or framebuffer?

 

Thomas

ラベル(1)
0 件の賞賛
返信
1 返信

1,124件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Thomas,

 

LPC178x MCUs include gray scale algorithms for STN displays only.  This provides 15 gray scales for monochrome displays.

 

Unfortunately, we do not have any gray scaler for TFT displays. In order to convert the colors you may use an external IC.

 

Sorry for the inconvenience this may cause you.

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信