Convert LPC1857 project to LPC1830

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Convert LPC1857 project to LPC1830

1,451件の閲覧回数
kensu
Contributor V

Hi,

I use LPC4330 EVA board to write application. But our target MCU is LPC1830,

What is the simplest way to convert to project to 1830, I try to change the MCU setting in project.

But after I change and want to flash with MCUXpresso IDE, it show "no flash configure" error message.

I don't know how to solve this.

Please give me some suggestions.

Thanks

Ken

pastedImage_1.png

pastedImage_2.png

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,354件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Ken Su,

   Actually, LPC1830 also have the according demo board, for example:NGX Xplorer LPC1830 board.

  I think, the most quick method is using the LPC1830 project, then add your modified application code.

  You can download the LPC1830 lpcopen code from this link:

http://www.nxp.com/downloads/en/software/lpcopen_3_01_lpcxpresso_ngx_xplorer_1830.zip

  There also have the freertos_blinky project.

 

Wish it helps you!

If you still have question, please let me know!

Have a great day,
Kerry

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信