I can't download software The USB Host Lite on the LPC2468. Please help me.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I can't download software The USB Host Lite on the LPC2468. Please help me.

406 Views
biswajitkundu
Contributor I

In my existing project (using LPC2468) I want to interface pen drive so please help me.

0 Kudos
1 Reply

276 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

As the USB Host Lite stack is from a couple of years ago, it just supports FAT16 file system. Nowadays is not common having new USB sticks in such format, as they came by default on FAT32 or exFAT file systems. It will be required using 3rd party software for formatting them on FAT16 (using Windows) or other applications like Gparted on Linux. It is mentioned on section 3 “Limitations” of AN10703:

http://www.nxp.com/docs/en/application-note/AN10703.pdf

You could find additional related information at the following link:

https://www.embeddedrelated.com/showthread/lpc2000/44451-1.php


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos