Connecting to LPC1769 Board Flashing through Commnad Prompt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connecting to LPC1769 Board Flashing through Commnad Prompt

1,016 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MaheshPrasath on Mon Dec 15 23:39:04 MST 2014
Hi
I need to flash two two LPC1769 board seperately connected to the same PC through command prompt. I am able to flash a singl board through the follwing commnad crt_emu_cm3_nxp -pLPC1769 -flash-load-exec=app.axf and it works fine as in the below link.

http://support.code-red-tech.com/CodeRedWiki/CommandLineFlashProgramming

Booting Problem

Booting LPC-Link

If using LPC-Link (the NXP LPCXpresso evaluation board debug probe) as your debug connection, first of all boot the LPC-Link
•
Under Windows, use the script
◦
bin\Scripts\bootLPCXpresso type
◾
where type = winusb for Windows XP, or type = hid for Windows Vista / 7.



Labels (1)
0 Kudos
Reply
1 Reply

1,005 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Dec 16 00:55:55 MST 2014
You have not asked a question, only made a statement...
0 Kudos
Reply