Connecting DS1307 To LPC1768 not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connecting DS1307 To LPC1768 not working

ソリューションへジャンプ
2,365件の閲覧回数
navidansari
Contributor III

hi

i connect ds1307 like this

1.png

battery is 3V and voltage on VCC is 5V . i connect another i2c device to i2c bus that its name is 24cxx 

24cxx vcc is 3.3 V . because its all open drain so i dont think it would be a problem to connect5 both of them to lpc1768

on keil for lpc1768 i connect to 24cxx and everything work right but when i try to connect to ds1307 its not happening

this is my code

#include "DS1307.h"
#include "Driver_I2C.h"
#include <string.h>
#include "cmsis_os.h"                   // ARM::CMSIS:RTOS:Keil RTX

/* I2C Driver */
extern ARM_DRIVER_I2C Driver_I2C0;
static ARM_DRIVER_I2C * DS1307I2Cdrv = &Driver_I2C0; 
 
#define DS1307_I2C_ADDR       0xD0      /* DS1307 I2C address         */

#define A_WR                  0         /* Master will write to the I2C       */
#define A_RD                  1         /* Master will read from the I2C      */

static uint8_t DS1307DeviceAddr;
static uint8_t DS1307_wr_buf[58];

void DS1307Init(){
     
     DS1307I2Cdrv->Initialize   (NULL);
  DS1307I2Cdrv->PowerControl (ARM_POWER_FULL);
  DS1307I2Cdrv->Control      (ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_STANDARD);
  DS1307I2Cdrv->Control      (ARM_I2C_BUS_CLEAR, 0);
     
     
     /* Init 24cxx EEPROM device */
  DS1307DeviceAddr = DS1307_I2C_ADDR;
     
     
     osDelay(100);
     unsigned char temp[1] = {0};
     DS1307_WriteBuf(0 , temp , 1); 
     

}

int32_t DS1307_ReadBuf (uint16_t addr, uint8_t *buf, uint32_t len) {
  uint8_t a[2];
 
  a[0] = (uint8_t)(addr >> 8);
  a[1] = (uint8_t)(addr & 0xFF);
 
  DS1307I2Cdrv->MasterTransmit (DS1307DeviceAddr, a, 2, true);
  while (DS1307I2Cdrv->GetStatus().busy);
  DS1307I2Cdrv->MasterReceive (DS1307DeviceAddr, buf, len, false);
  while (DS1307I2Cdrv->GetStatus().busy);
  if (DS1307I2Cdrv->GetDataCount () != len) return -1;
 
  return 0;
}


int32_t DS1307_WriteBuf (uint16_t addr, const uint8_t *buf, uint32_t len) {
 

     
  DS1307_wr_buf[0] = (uint8_t)(addr >> 8);
  DS1307_wr_buf[1] = (uint8_t)(addr & 0xFF);
 
  memcpy (&DS1307_wr_buf[2], &buf[0], len);
 
  DS1307I2Cdrv->MasterTransmit (DS1307DeviceAddr, DS1307_wr_buf, len + 2, false);
  while (DS1307I2Cdrv->GetStatus().busy);
  if (DS1307I2Cdrv->GetDataCount () != (len + 2)) return -1;
  /* Acknowledge polling */
 
  do {
    DS1307I2Cdrv->MasterReceive (DS1307DeviceAddr, &DS1307_wr_buf[0], 1, false);
    while (DS1307I2Cdrv->GetStatus().busy);
  } while (DS1307I2Cdrv->GetDataCount () < 0);
 
  return 0;
}
‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

in logic analyzer i just recieve this

2.png

why i cant read or write anything to it?

its my main code

     DS1307Init();
     

     
     
     
     osDelay(100);
     state = DS1307_ReadBuf(0,mTime,1);‍‍‍‍‍‍‍‍
ラベル(3)
タグ(3)
1 解決策
2,046件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi navid ansari,

Thanks for reply.

Firstly, I think the hardware circuit is correct, and I've attached a DS1302 driver.

Please refer to it for details.

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,047件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi navid ansari,

Thanks for reply.

Firstly, I think the hardware circuit is correct, and I've attached a DS1302 driver.

Please refer to it for details.

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------