Config Tools New Project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Config Tools New Project

1,603 次查看
denjos007
Contributor II

Hi, 

I am planning to use an LPC55S69 board for a project and I am used to developing firmware in CLion. So the natural toolchain was to use config tools to create new projects and use ARM GCC for compiling. This works well when using the existing example to create new projects, however, if i want to use driver components not part of the example, config tools complains that there are no corresponding drivers in the toolchain project. 

Is there a way to create projects with the required tools in config tools or any other online tools that can accomplish this? I know the functionality exists in MCUXpressoIDE, but I want to bypass using that in the workflow.

Thanks in advance

标记 (2)
0 项奖励
回复
2 回复数

1,580 次查看
denjos007
Contributor II

I would like to cut out using MCUXpresso IDE. Also the files created with MCUXpressoIDE does not come with corresponding CMake files to use directly in the standalone ARM GCC development. 

Is there such a tool to create new projects outside MCUXpresso IDE? 

Also is there a document on the expected folder structure for the toolchain project expected by config tools? If such a tool is not present, then  I could at least try manually copying the driver source to the project.

0 项奖励
回复

1,584 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suggest you use MCUXpresso IDE to create a new project based on SDK for LPC family.

BR

XiangJun Rong

0 项奖励
回复