Concerning the ADC of the LPC1549JBD64: Is it possible to measure an analog voltage on ADC0_1 and ADC1_0 simultaneously, or can it only be done sequentially?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Concerning the ADC of the LPC1549JBD64: Is it possible to measure an analog voltage on ADC0_1 and ADC1_0 simultaneously, or can it only be done sequentially?

794 Views
maxveen
Contributor I

Simultaneous measurements on ADCchannels of LPC1549 

0 Kudos
Reply
1 Reply

678 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Max Veen,

Thank you for your interest in NXP Semiconductor products and  the opportunity to serve you.Is 

it possible to measure an analog voltage on ADC0_1 and ADC1_0 simultaneously, or can it only be done sequentially?
--- Yes, they can sample the signals simultaneously.

Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply