Concerning the ADC of the LPC1549JBD64: Is it possible to measure an analog voltage on ADC0_1 and ADC1_0 simultaneously, or can it only be done sequentially?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Concerning the ADC of the LPC1549JBD64: Is it possible to measure an analog voltage on ADC0_1 and ADC1_0 simultaneously, or can it only be done sequentially?

789件の閲覧回数
maxveen
Contributor I

Simultaneous measurements on ADCchannels of LPC1549 

0 件の賞賛
返信
1 返信

673件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Max Veen,

Thank you for your interest in NXP Semiconductor products and  the opportunity to serve you.Is 

it possible to measure an analog voltage on ADC0_1 and ADC1_0 simultaneously, or can it only be done sequentially?
--- Yes, they can sample the signals simultaneously.

Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信