Clarification questions on SGPIO for LPC 43XX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Clarification questions on SGPIO for LPC 43XX

1,610件の閲覧回数
marvincabuenas
Contributor II

Hello NXP,

I want to clarify a few things regarding the SGPIO for LPC 43XX.

  1. When using the slice mux cfg register, is there a way to invert the external input clock?
  2. When using a qualifier for sgpio mux cfg register, is there a way to only use it once on a periodic signal? This means, we only want to use the qualifier on the first detection of an input slice.

3. We have a loopback set-up in our board. SGPIO 8 serves as a clock input of SGPIO 0 and SGPIO 1. SGPIO 10 serves as data input to SGPIO 1. We set-up the slice corresponding to SGPIO 1 clk capture mode to use the rising clock edge, so that we can save the data at the falling edge. However, for some reason, this behavior is not seen in my tests on my board. The performance varies between runs.

ラベル(1)
0 件の賞賛
返信
1 返信

1,578件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @marvincabuenas 

1)Try to configure as below:

Alice_Yang_0-1689130938556.pngAlice_Yang_0-1689130938556.png

2) The qualifier can be Disable by setting QUALIFIER_MODE=1, resulting in no shift_clk.

3) About this question, recommend you refer to 

20.8.1.1 I2S slice selection of user manual, and some application notes about SGPIO:

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...   

 

BR

Alice

 

 

0 件の賞賛
返信