Hi, Jim,
I suggest you download the SDK package from the link:
MCUXpresso SDK | Software Development for Kinetis, LPC, and i.MX MCUs | NXP
On the package, there is example in the directory:
C:\DriveE\LPC_SDK_MCUExpresso\SDK_2.6.0_LPCXpresso804\boards\lpcxpresso804\demo_apps\power_mode_switch_lpc
This is part of the code
void POWER_EnterDeepSleep(uint32_t activePart)
{
assert((SYSCON->MAINCLKSEL & SYSCON_MAINCLKSEL_SEL_MASK) == 0U);
uint32_t pmsk;
pmsk = __get_PRIMASK();
__disable_irq();
PMU->PCON = (PMU->PCON & (~PMU_PCON_PM_MASK)) | PMU_PCON_PM(kPmu_Deep_Sleep);
/* remain active during power down mode */
SYSCON->PDSLEEPCFG &= ~activePart;
/* enable Deepsleep mode in the ARM-CORTEX M0+ SCR register */
SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;
/* Enter powerdown mode */
__WFI();
/* disable Deepsleep mode in the ARM-CORTEX M0+ SCR register */
SCB->SCR &= ~SCB_SCR_SLEEPDEEP_Msk;
__set_PRIMASK(pmsk);
}
If you want to wake-up from Pin intrrupt, you can refer to the code:
static void DEMO_InitWakeupPin(void)
{
gpio_pin_config_t gpioPinConfigStruct;
/* Set SW pin as GPIO input. */
gpioPinConfigStruct.pinDirection = kGPIO_DigitalInput;
GPIO_PinInit(DEMO_USER_WAKEUP_KEY_GPIO, DEMO_USER_WAKEUP_KEY_PORT, DEMO_USER_WAKEUP_KEY_PIN, &gpioPinConfigStruct);
SYSCON_AttachSignal(SYSCON, kPINT_PinInt0, DEMO_PINT_PIN_INT0_SRC);
/* Configure the interrupt for SW pin. */
PINT_Init(PINT);
PINT_PinInterruptConfig(PINT, kPINT_PinInt0, kPINT_PinIntEnableFallEdge, pint_intr_callback);
PINT_EnableCallback(PINT); /* Enable callbacks for PINT */
}
Hope it can help you
BR
XiangJun Rong