Can't Build lpc_open examples for LPC1857 using Keil

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't Build lpc_open examples for LPC1857 using Keil

1,271 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dsidlauskas on Wed Feb 05 17:57:04 MST 2014
I hope this is the right place to post this.

I am using Keil uvision 5.1 and lpc_open for keil lpc1857.

Following the quick start guide I loaded the peripheral example projects into uvision.

The 2 libraries build with no problem, but when I try to build any of the examples I immediately get the error:

Error: *** Device is not supported by Toolchain ! ***

Does anyone have a clue?

Thanks,
Dave Sidlauskas
Labels (1)
0 Kudos
Reply
2 Replies

1,257 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dsidlauskas on Thu Feb 06 08:52:05 MST 2014
Thanks for the advice. Problem solved: It was a licensing issue.
0 Kudos
Reply

1,257 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Wed Feb 05 20:20:15 MST 2014
Hi David,
If you are not seeing device from device tab you may need to install legacy pack from
http://www2.keil.com/mdk5/legacy
0 Kudos
Reply