Can't Build lpc_open examples for LPC1857 using Keil

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't Build lpc_open examples for LPC1857 using Keil

1,257件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dsidlauskas on Wed Feb 05 17:57:04 MST 2014
I hope this is the right place to post this.

I am using Keil uvision 5.1 and lpc_open for keil lpc1857.

Following the quick start guide I loaded the peripheral example projects into uvision.

The 2 libraries build with no problem, but when I try to build any of the examples I immediately get the error:

Error: *** Device is not supported by Toolchain ! ***

Does anyone have a clue?

Thanks,
Dave Sidlauskas
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,243件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dsidlauskas on Thu Feb 06 08:52:05 MST 2014
Thanks for the advice. Problem solved: It was a licensing issue.
0 件の賞賛
返信

1,243件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Wed Feb 05 20:20:15 MST 2014
Hi David,
If you are not seeing device from device tab you may need to install legacy pack from
http://www2.keil.com/mdk5/legacy
0 件の賞賛
返信