Can i use SPI on development board or do i have to use SPIFI?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can i use SPI on development board or do i have to use SPIFI?

802 Views
blair_smyth
Contributor I

Hi there,

I am currently using the LPCxpresso546 development board. I was just wondering is it possible to talk to the W25Q128JVFIM FLASH chip through SPI alone and without using SPIFI?

Kind regards,

Blair

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

737 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello Blair,

Hope you are doing well.

Yes it is possible to interface with standard SPI. Checking the datasheet of the part number you have provided it supports the following including SPI.

pastedImage_1.png

Please note that the SPIFI focuses on interface with SPI flash only, the SPI is an interface which can connect to a lot devices including flash.

Hope it helps!

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos
Reply