Can i use SPI on development board or do i have to use SPIFI?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can i use SPI on development board or do i have to use SPIFI?

796件の閲覧回数
blair_smyth
Contributor I

Hi there,

I am currently using the LPCxpresso546 development board. I was just wondering is it possible to talk to the W25Q128JVFIM FLASH chip through SPI alone and without using SPIFI?

Kind regards,

Blair

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

731件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello Blair,

Hope you are doing well.

Yes it is possible to interface with standard SPI. Checking the datasheet of the part number you have provided it supports the following including SPI.

pastedImage_1.png

Please note that the SPIFI focuses on interface with SPI flash only, the SPI is an interface which can connect to a lot devices including flash.

Hope it helps!

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 件の賞賛
返信