Can fd interface in LPC54000 series MCU is iso version or not?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can fd interface in LPC54000 series MCU is iso version or not?

1,160 Views
chenyandong
Contributor II

The MCAN controller is designed to provide a full implementation of the CAN protocol according to the CAN Specification Version 2.0 part A and to CAN FD Specification V.1.0

CAN FD Specification V.1.0:ISO CAN FD or non-ISO CAN FD?

Thank you!

Labels (1)
0 Kudos
Reply
1 Reply

931 Views
soledad
NXP Employee
NXP Employee

Hi,

In the control register (CCCR) you can select ISO or Non ISO operation. Please check the LPC546xx user manual, Table 713, for more information.

https://www.nxp.com/docs/en/user-guide/UM10912.pdf 

pastedImage_2.png


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------