Can fd interface in LPC54000 series MCU is iso version or not?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can fd interface in LPC54000 series MCU is iso version or not?

1,248件の閲覧回数
chenyandong
Contributor II

The MCAN controller is designed to provide a full implementation of the CAN protocol according to the CAN Specification Version 2.0 part A and to CAN FD Specification V.1.0

CAN FD Specification V.1.0:ISO CAN FD or non-ISO CAN FD?

Thank you!

ラベル(1)
0 件の賞賛
返信
1 返信

1,019件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

In the control register (CCCR) you can select ISO or Non ISO operation. Please check the LPC546xx user manual, Table 713, for more information.

https://www.nxp.com/docs/en/user-guide/UM10912.pdf 

pastedImage_2.png


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------