Can LPC802 IO support 5V voltage pull high

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can LPC802 IO support 5V voltage pull high

1,225 Views
li-chinwang
Contributor II

Customer plan to use LPC802 to connect to an 5V CODEC via 5V pull up I2C.

Since LPC802/804 input can support max 5.4V voltage, can customer do so in HW without level shift?

0 Kudos
Reply
1 Reply

1,137 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
It's necessary to need a level shift in this implementation, just in case.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply