Can LPC55S69 run 1.8V GPIO/UART ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can LPC55S69 run 1.8V GPIO/UART ?

1,452件の閲覧回数
dav1
Contributor V

hi,

The datasheet for LPC55S69JEV98K states VDD 'main io supply', min 1.8V

does that mean 1.800V ? 
i.e. most buck regulators would have about 3-5% output tolerance, meaning the VDD rail and serial IO might as well be 1.72V.

 

Is the datasheet correct, i.e. 1.8V is absolute minimum? or can you run the LPC55-series safely in a 1.8V system?

 

thx

 

ラベル(1)
0 件の賞賛
返信
1 返信

1,433件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi dav1 

Yes LPC55S69 VDD absolute minimum is 1.8V. We can guarantee the part work safe with 1.8V.

 We can't guarantee operation normal with  1.72V VDD.

Thanks,

Jun Zhang

0 件の賞賛
返信