LPC435X USBD_HW_API::ReadReqEP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC435X USBD_HW_API::ReadReqEP

ソリューションへジャンプ
2,449件の閲覧回数

Hi,

Is it safe to call "USBD_HW_API::ReadReqEP" , that is function in LPC4357 USB API, at a different timing than sample code?
For example, we want to use this function in the below sequence.
(1)call "USBD_HW_API::ReqdReqEP" when recieved "NOTIFY_TRANSFER_DATA_SIZE" the vendor request
(2)start to transfer bulk out

The reference materials are as follows.
sample1:TN00041\usbdlib_for_LPC43xx.Release\usbdlib_for_LPC43xx.Release\usbd_lib_lpc43xx\examples_43xx_18xx\usbd_lib_cdc_uart\src\cdc_uart.c
sample2:TN00041\usbdlib_for_LPC43xx.Release\usbdlib_for_LPC43xx.Release\usbd_lib_lpc43xx\examples_43xx_18xx\usbd_lib_libusb\src

In the sample code, call "USBD_HW_API::ReqdReqEP" timing is
sample1:USB_EVT_OUT_NAK (Bulk Out NAK Interrupt)
sample2:USB_EVT_OUT (Bulk Out RecieveEnd Interrupt)

We checked the specification documents, but the information of call function timing is nothing.
・UM10503.pdf/27.5.34 USBD_HW_API/Table 595. USBD_HW_API class structure(P813)
・TN00041/usbdlib_for_LPC43xx.Release/usbdlib_for_LPC43xx.Release/usbd_lib_lpc43xx/LPC_USBD_Lib/docs/html/struct_u_s_b_d___h_w___a_p_i___t.html

0 件の賞賛
返信
1 解決策
2,425件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

ReadReqEP() sets up the DMA descriptors in preparation for transferring data from memory to the USB controller. Then it primes the endpoint.

ReadEP() only returns the total bytes transferred once the DMA operation is complete. It does nothing with the data buffer pointer passed in.

NAKs are the throttling mechanism on a USB bus. If the CPU is slower at generating data that the USB is at shipping it out then NAKs provide a convenient and legal way to tell the host to wait for more data to arrive.

The best way to call these functions is:

Call ReadReqEP() once to get the stream started

Call ReadEP() following the receipt of an IN completion, then call ReadReqEP() to get the next transfer started.

Call ReadReqEP() any time a NAK is received.

Thanks,

Jun Zhang

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,397件の閲覧回数

Thanks for the support. I understand it.

0 件の賞賛
返信
2,426件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

ReadReqEP() sets up the DMA descriptors in preparation for transferring data from memory to the USB controller. Then it primes the endpoint.

ReadEP() only returns the total bytes transferred once the DMA operation is complete. It does nothing with the data buffer pointer passed in.

NAKs are the throttling mechanism on a USB bus. If the CPU is slower at generating data that the USB is at shipping it out then NAKs provide a convenient and legal way to tell the host to wait for more data to arrive.

The best way to call these functions is:

Call ReadReqEP() once to get the stream started

Call ReadEP() following the receipt of an IN completion, then call ReadReqEP() to get the next transfer started.

Call ReadReqEP() any time a NAK is received.

Thanks,

Jun Zhang

0 件の賞賛
返信