Can I only use the M0 core with LPC54114?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I only use the M0 core with LPC54114?

1,431 Views
da_chen
Contributor II

I found many examples about how to use dual cores. But no one said how to only use the M0 core to work. Is this possible?

Labels (1)
Tags (2)
1 Reply

1,330 Views
brendonslade
NXP TechSupport
NXP TechSupport

The LPC5411x is intended for the M4 to release the M0+ since the M0+ is primarily there as a slave core, so the examples are geared up for this.

If you are looking for an M0+ only device with the same / very similar peripherals I'd suggest using the LPC51U68, which is a lower cost.