CRC32 with LPC1788

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,206件の閲覧回数
erenaud
Contributor II

Hello everyone !

I am currently trying to compute CRC32 checksum with a LPC1788.

Here is the functions I am using :

 

#define u32      unsigned long

void Reg_InitCRC()
{
/* Standard CRC32 */
   CRC_MODE = 0x00000036;
/* CRC32 MPEG-2 */
//   CRC_MODE = 0x00000002;
   CRC_SEED = 0xFFFFFFFF;
}

u32 REG_Calculate_CRC(u32 u32_Data)
{
   u32 u32_CRC;
   CRC_WR_DATA = u32_Data;
   u32_CRC = CRC_SUM;
   return u32_CRC;
}

 

 Then, I am testing those function with this code :

 

u32 u32_data[4];
   u32_data[0] = 0xAAAAAAAA;
   u32_data[1] = 0x69686968;
   u32_data[2] = 0x69686869;
   u32_data[3] = 0x12345678;

   u32 u32_res = 0;

   Reg_InitCRC();
   u32_res = REG_Calculate_CRC(u32_data[0]);
   CRC_SEED = 0xFFFFFFFF; // Not really needed, just for safety
   u32_res = REG_Calculate_CRC(u32_data[1]);
   CRC_SEED = 0xFFFFFFFF;
   u32_res = REG_Calculate_CRC(u32_data[2]);
   CRC_SEED = 0xFFFFFFFF;
   u32_res = REG_Calculate_CRC(u32_data[3]);

 

So when doing this, I am observing a really strange behavior. When the input data is an u32 composed of identicals u8 (example : 0xAAAAAAAA) or "symetrical" u8 (0x12343412 and 0x69686869) the CRC output is correct (for both CRC32 and CRC32-MPEG2).
But when the data input is made of differents u8 (example : 0x12345678), the output is not what I am expecting at all.

Here's a table summing up my situation :

InputMy CRC32 outputReal CRC32 outputMy MPEG2 outputReal MPEG2 output
0xAAAAAAAA0xb596e05e0xB596E05E0x42fc4b290x42FC4B29
0x123434120xb0a58ffb0xB0A58FFB0x9db25e0f0x9DB25E0F
0x696868690xb8e4c55e0xB8E4C55E0xff43f3da0xFF43F3DA
0x123456780xaf6d87d20x4A090E98 0xad37d0560xDF8A8A2B

 

When looking at this table, I finnally understood : if I want to have the "expected" CRC32, I have to reverse bytes (and not bits) in my input. So for the last line :

0x78563412 in my code (but actually computing CRC32 for 0x12345678)0x4a090e980x4A090E980xdf8a8a2b0xDF8A8A2B


So my question is : why do I have to switch the endianess of my u32 to find the expected result ?

Note : I am using this website to check CRC32.

0 件の賞賛
返信
1 解決策
4,187件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that the CRC module of LPC1788 uses big endian format.

With PC CRC tools, if you input 0x78563412, the CRC32 output will be 0xaf6d87d2

With LOPC1788, if you input 0x12345678, the CRC32 output will be 0xaf6d87d2.

In conclusion, the CRC module of LPC1788 use big endian.

Hope it can help you

BR

XiangJun Rong

元の投稿で解決策を見る

3 返答(返信)
4,188件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that the CRC module of LPC1788 uses big endian format.

With PC CRC tools, if you input 0x78563412, the CRC32 output will be 0xaf6d87d2

With LOPC1788, if you input 0x12345678, the CRC32 output will be 0xaf6d87d2.

In conclusion, the CRC module of LPC1788 use big endian.

Hope it can help you

BR

XiangJun Rong

4,198件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi

How about using the init function:

void Reg_InitCRC()
{
/* Standard CRC32 */
   CRC_MODE = 0x00000032; //instead of 0x36
/* CRC32 MPEG-2 */
//   CRC_MODE = 0x00000002;
   CRC_SEED = 0xFFFFFFFF;
}

I think that the BIT_RVS_WR should be cleared rather than being set.

xiangjun_rong_0-1623296166526.png

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信
4,191件の閲覧回数
erenaud
Contributor II

Hi,
First of all, thank you for your answer.
I think I already tried that, I will double check this afternoon.

But if I understand the documentation clearly, what BIT_RVS_WR is doing is reversing the bits order (and not the bytes).
So, 0x1234 5678 will be treated as 0x1E6A 2C48, am I right ?

(in binary)
00010010 00110100 01010110 01111000 --> 00011110 01101010 00101100 01001000

0 件の賞賛
返信