CRC Engine on LPC54xx/S0xx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CRC Engine on LPC54xx/S0xx

1,110 Views
ceso
Contributor I

Hello, are the only compatible CRC's for the CRC engine the three CRCs that are in the datasheet? Or will additional CRCs need to be implemented by using user-developed software that will not run in the engine? Additionally, does it support 8-bit CRCs

 

0 Kudos
Reply
1 Reply

1,092 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

1) "are the only compatible CRC's for the CRC engine the three CRCs that are in the datasheet? Or will additional CRCs need to be implemented by using user-developed software that will not run in the engine?"

->> YES.

2) Accept any size of data width per write: 8, 16 or 32-bit.

 

BR

Alice

0 Kudos
Reply