CAN Basic mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN Basic mode

2,179件の閲覧回数
ianbenton
Senior Contributor I

Section 27.7.2.4.4. of the LPC15xx manual states:

"The transmission of the contents of the
IF1 Registers is requested by writing the BUSY bit of the IF1 Command Request Register
to ‘1’."

Table 403 states that bit 15 (the BUSY bit) of IF1_CMDREQ is read-only.

Please clarify.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,959件の閲覧回数
ianbenton
Senior Contributor I

That code writes to bit 15, which the manual says is read-only?

0 件の賞賛
返信

1,959件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi  Ian Benton,

It's typo with reference manual.

Hope this is clear.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,959件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi  Ian Benton,

Thank you for your interest in NXP Semiconductor products and 
the opportunity to serve you.

You can use the following code to set the BUSY bit in the Command Request Register.

#define IFCREQ_BUSY    0x8000    /* 1 is writing is progress, cleared when 
LPC_CAN->IF2_CMDREQ = IFCREQ_BUSY;    /* Start message transfer */
Have a great day,
TIC
 
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信