Bootstrap Loader for LPC4357

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bootstrap Loader for LPC4357

950 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mpkahroba on Fri Oct 12 07:10:51 MST 2012
Hello Everyone
I need a bootstrap loader which loads the program from internal ROM of LPC4357 into SRAM Connected to EMC, I want to use External SRAM to execute the code from, and to keep LCD Frame buffer and use the internal SRAM to keep data. I need the way to do shadowing and want to know how much could be the maximum frequency of the EMC bus.
标签 (1)
0 项奖励
回复
0 回复数