Bootstrap Loader for LPC4357

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bootstrap Loader for LPC4357

949件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mpkahroba on Fri Oct 12 07:10:51 MST 2012
Hello Everyone
I need a bootstrap loader which loads the program from internal ROM of LPC4357 into SRAM Connected to EMC, I want to use External SRAM to execute the code from, and to keep LCD Frame buffer and use the internal SRAM to keep data. I need the way to do shadowing and want to know how much could be the maximum frequency of the EMC bus.
ラベル(1)
0 件の賞賛
返信
0 返答(返信)