Bootloader for LPC546XXX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bootloader for LPC546XXX

2,993件の閲覧回数
salmansattar
Contributor II

Hello Everyone,

I am looking for custom bootloader for LPC 32-bit ARM(MCUs - lpc546XXX). I would like to have two separate images stored in program flash and let bootloader decide which image to load. 

I do not have any starting point for that and there is no example that i can follow. I would appreciate any help.

Thank in advance

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,708件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Salman sattar,

    If you want to have two separate image stored in Pflash, you need to create the secondary bootloader to download and choose the according app code.

   But, now we still don't have the secondary bootloader code for LPC5460X, so you need to create it by yourself.

   After I search the website, I found a secondary bootloader for LPC54102, I think it may useful to you:

http://cache.nxp.com/docs/en/application-note/AN11610.zip?fsrch=1&sr=3&pageNum=1 


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,708件の閲覧回数
salmansattar
Contributor II

Thank you i will try this out

0 件の賞賛
返信