Booting LPC55 via I2C, can we trigger flash-boot via rom-loader?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Booting LPC55 via I2C, can we trigger flash-boot via rom-loader?

1,658 Views
dav1
Contributor V

When using the built-in I2C "ISP boot mode" of the LPC55 series cpu's
is it possible for the host to signal via I2C to immediately exit the rom based bootloader to continue booting via flash?

 

I don't have the option to add a dedicated gpio to control ISP, so idea was to always enter the rom boot mode -> read flash region to check installed firmware -> if up to date -> continue to boot via flash

 

doable?

0 Kudos
Reply
3 Replies

1,633 Views
dav1
Contributor V

thanks, sounds good!

do you have an idea of how long it will take to run these commands over i2c?

i couldn't find any wait times in the datasheet so should be fairly instant (i hope)

 

0 Kudos
Reply

1,641 Views
jay_heng
NXP Employee
NXP Employee

Yes, you can try read-memory and execute commands in UM 8.9.5 I2C ISP commands

Use read-memory command to read back app data from internal flash

Use execute command to jump to app

0 Kudos
Reply

1,318 Views
dav1
Contributor V

having trouble with this, the UM 8.9.5 doesn't have an example so tried this:

boot_cmd[22] = {0x5A,0xA4,0x10,0x00,0x00,0x00,0x09,0x00,0x00,0x03,0x6c,0x01,0x00,0x00,0x00,0x80,0x01,0x20,0x00,0x80,0x01,0x20}
 
where 0x09 is the execute cmd, but the response code is command not supported
0 Kudos
Reply