Bit band mapping on LPC5410x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bit band mapping on LPC5410x

ソリューションへジャンプ
2,197件の閲覧回数
rogerlittlewood
Contributor I

LPC5410x

There seems to be little info about using bit-banding on this device. Where can I find this information, for example mapping between the bit-band area and specific peripheral register bits? Which peripherals use bit-banding?......

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,999件の閲覧回数
ckphua
NXP Employee
NXP Employee

Hi,

LPC5410x User Manual did not describe this (and we will update in the next version). Meantime the LPC5410x Bit-band region is (0x4000 0000 to 0x40100000) can be accessed in the so-called alias region at 0x4200 0000.

This means all the APB Peripherals are mapped in the bit-band region.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,000件の閲覧回数
ckphua
NXP Employee
NXP Employee

Hi,

LPC5410x User Manual did not describe this (and we will update in the next version). Meantime the LPC5410x Bit-band region is (0x4000 0000 to 0x40100000) can be accessed in the so-called alias region at 0x4200 0000.

This means all the APB Peripherals are mapped in the bit-band region.

0 件の賞賛
返信
1,999件の閲覧回数
rogerlittlewood
Contributor I

Thanks. So I hope the new version comes out soon so we can start to use those clever features thoughtfully provided by the ARM system designers!

0 件の賞賛
返信