Bit band mapping on LPC5410x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bit band mapping on LPC5410x

Jump to solution
2,187 Views
rogerlittlewood
Contributor I

LPC5410x

There seems to be little info about using bit-banding on this device. Where can I find this information, for example mapping between the bit-band area and specific peripheral register bits? Which peripherals use bit-banding?......

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,989 Views
ckphua
NXP Employee
NXP Employee

Hi,

LPC5410x User Manual did not describe this (and we will update in the next version). Meantime the LPC5410x Bit-band region is (0x4000 0000 to 0x40100000) can be accessed in the so-called alias region at 0x4200 0000.

This means all the APB Peripherals are mapped in the bit-band region.

View solution in original post

0 Kudos
Reply
2 Replies
1,990 Views
ckphua
NXP Employee
NXP Employee

Hi,

LPC5410x User Manual did not describe this (and we will update in the next version). Meantime the LPC5410x Bit-band region is (0x4000 0000 to 0x40100000) can be accessed in the so-called alias region at 0x4200 0000.

This means all the APB Peripherals are mapped in the bit-band region.

0 Kudos
Reply
1,989 Views
rogerlittlewood
Contributor I

Thanks. So I hope the new version comes out soon so we can start to use those clever features thoughtfully provided by the ARM system designers!

0 Kudos
Reply