.BSDL files for LPC1833JET256,LPC1833FET256...

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

.BSDL files for LPC1833JET256,LPC1833FET256...

2,067件の閲覧回数
jFidrich
Contributor I

Good day,

I am searching for .bsdl files for these models of MCUs. I found some for FET models f.e. lpc4357fet256_rev-_20130527-v2.bsd, but none for LPC43S6, LPC43S5... nad JET models(different temperature range) and LPC4333JEF/FET etc.

Here is complete list:

LPC1833JET256,LPC1833FET256,LPC4333JET256 ,LPC4333FET256,LPC1837JET256,LPC1857FET256,LPC18S57JET256,LPC1857JET256,LPC1837FET256,LPC43S57JET256,LPC4357FET256,LPC4357JET256,LPC4337JET256,LPC4337FET256,LPC43S67JET256

Thank you!

With Best Regards,

J.Fidrich

 

ラベル(2)
0 件の賞賛
返信
4 返答(返信)

2,045件の閲覧回数
jFidrich
Contributor I

Thank you Miguel,

I've found these files even before I started this topic. Problem is that if I click f.e. on LPC43S67 ... complete name LPC43S67JBD208 there are files with this name conventions - lpc43x0fet256_revA-20130527-v2.bsd or LPC18xx_43xx BSDL files lpc43x0fbd208_revC_20130527-v2.bsd and for lets say "JBD" there are no files and there are other variations in names of these MCUs.
To have better picture of my situation I am preparing JTAG infrastructure test which calls IDCODE of MCU and compares if there is part in compliance with BOM. If we can proove that all MCUs I mentioned has same IDs or there are .bsd files which contains information for lets say 18xx and 43xx only and only these differ in ID code then everything is fine. If these IDs will not be same we will have problems failing on infrastructure test.

With Best Regards,

jFidrich

0 件の賞賛
返信

2,023件の閲覧回数
Miguel04
NXP TechSupport
NXP TechSupport

Hi @jFidrich 

If the part number is not specified you could look for the Package number and use the same BSDL.

f.e.

The JBD has a package of LQFP208 and the FBD has also LQFP208.

Best Regards, Miguel.

0 件の賞賛
返信

2,005件の閲覧回数
jFidrich
Contributor I

Thanks for your response Miguel,

I downloaded two .bsdl files from same package.

lpc18x0fet256_revA_20130527-v2.bsd

lpc43x0fet256_revA-20130527-v2.bsd

These files has different parameter ID CODE.

-- Description : BSDL file for LPC43x0FET256 (LBGA256 package)
-- Silicon revision A
-- IDCODE: 0x5906002B

-- Description : BSDL file for LPC18x0FET256 (LBGA256 package)
-- Silicon revision A
-- IDCODE: 0x5284E02B

So I will probably need .bsdl files for all listed MCUs as they have different parameter IDCODE.

I am running out of time to provide solution so I started support ticket also. 

Thanks for your help,

Best Regards,

jfidrich

0 件の賞賛
返信

2,051件の閲覧回数
Miguel04
NXP TechSupport
NXP TechSupport

Hi @jFidrich 

You can find the BSDL files on the main page of MCU, f.e. this link take you to the LPC43S67,  go to Documentation and Design resources and you will find the BSDL file.

Let me know if you have another question.

Best Regards, Miguel.

0 件の賞賛
返信