BOD reset level

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,123件の閲覧回数
peterwöß-krausb
Contributor I

Hello,

table 21 in the datasheet LPC11U6x / Rev. 1.3. shows the characteristics for the 

interrupt level 2 & 3, and for reset level 2 & 3.

What are the characteristics for reset level 0 & 1, as table 58 / document UM10732 

allows BOD reset level 0, 1, 2, 3.

Best regards, 

Peter

ラベル(1)
0 件の賞賛
返信
1 解決策
1,941件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi Peter,

On the LPC11U6x, those levels are not there since the assertion points are below the minimum operating Vdd voltage.

 only levels mentioned in the datasheet are workable thresholds available.

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,942件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi Peter,

On the LPC11U6x, those levels are not there since the assertion points are below the minimum operating Vdd voltage.

 only levels mentioned in the datasheet are workable thresholds available.

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,941件の閲覧回数
peterwöß-krausb
Contributor I

thx

0 件の賞賛
返信