BOD reset level

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BOD reset level

Jump to solution
2,122 Views
peterwöß-krausb
Contributor I

Hello,

table 21 in the datasheet LPC11U6x / Rev. 1.3. shows the characteristics for the 

interrupt level 2 & 3, and for reset level 2 & 3.

What are the characteristics for reset level 0 & 1, as table 58 / document UM10732 

allows BOD reset level 0, 1, 2, 3.

Best regards, 

Peter

Labels (1)
0 Kudos
Reply
1 Solution
1,940 Views
soledad
NXP Employee
NXP Employee

Hi Peter,

On the LPC11U6x, those levels are not there since the assertion points are below the minimum operating Vdd voltage.

 only levels mentioned in the datasheet are workable thresholds available.

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,941 Views
soledad
NXP Employee
NXP Employee

Hi Peter,

On the LPC11U6x, those levels are not there since the assertion points are below the minimum operating Vdd voltage.

 only levels mentioned in the datasheet are workable thresholds available.

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,940 Views
peterwöß-krausb
Contributor I

thx

0 Kudos
Reply