BOD implementation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

BOD implementation

跳至解决方案
3,239 次查看
timokunze
Contributor I

Hello,

do you have a example implementation for BOD LPC4317?  

I wrote the following lines:

  // Bown-Out Detect voltage level (0-3)
  uint32_t bodVoltageLevel = 3; // interrupt level 3 (3.05V)
  // Brown-Out Reset voltage level (0-3)
  uint32_t borVolatgeReset = 0; // reset level 0 (1.9V)
 
 NVIC_DisableIRQ(EVENTROUTER_IRQn);
 
 // Initialize the event router.
 Chip_EVRT_Init();
 
 // Configures the BOD level and reset level on LPC18xx/LPC43xx parts.
 // Note: BOD reset is not used!
 Chip_CREG_ConfigureBODaR(bodVoltageLevel, borVolatgeReset);
   
 // Set up the type of interrupt type for a source to EVRT.
 // Level configuration register (HILO)
 // Edge configuration (EDGE)
 // HILO bit  n EDGE bit n  Description
  // 0      0       Detect LOW level (currently active)
  // 0      1       Detect falling edge
  // 1      0       Detect HIGH level
  // 1      1       Detect rising edge 
  Chip_EVRT_ConfigIntSrcActiveType(EVRT_SRC_BOD1, EVRT_SRC_ACTIVE_LOW_LEVEL); 
  
 // *** 
 // Event Enable register (ENABLE)
 // The ENABLE register can be read at any time. To change the contents of this register, use
  // the CLR_EN and SET_EN registers.
 
 // Set event enable register (SET_EN)
 // The SET_EN register sets the corresponding bits in the ENABLE register.
 // Enable interrupt sources to EVRT. Source is BOD.
 // BOD interrupt. Not active in Deep-sleep, Power-down, and
  // Deep power-down mode. Use for wake-up from Sleep mode.
 // Note: BOD reset is not used!
 Chip_EVRT_SetUpIntSrc(EVRT_SRC_BOD1, ENABLE);

 // Clear event enable register (CLR_EN)
  // The CLR_EN register clears the corresponding bits in the ENABLE register.
 // Nothing to do.

  // ***
  // Event status register (STATUS)
 // The STATUS register monitors the internally generated interrupt or event signal from the
 // peripherals. The contents of this register can be read at any time. To change the contents
 // of this register, use the CLR_STAT and SET_STAT registers. 
 
 // Set event status register (SET_STAT)
 // Nothing to do.
 
 // Clear event status register (CLR_STAT)
 // Clear pending interrupt EVRT source. Source is BOD.
 Chip_EVRT_ClrPendIntSrc(EVRT_SRC_BOD1); 

 // ***
  // Set irq event router priority
  NVIC_SetPriority(EVENTROUTER_IRQn, 1); // High priority 
 // Clear a pending event router interrupt
  NVIC_ClearPendingIRQ(EVENTROUTER_IRQn);
 // Enable event router interrupt
  NVIC_EnableIRQ(EVENTROUTER_IRQn);

The IRQ Looks like:

void EVRT_IRQHandler(void)
{
 // For debugging, remove later again
 __nop();
 
 // Check if a source is sending interrupt to EVRT 
 if (SET == Chip_EVRT_IsSourceInterrupting(EVRT_SRC_BOD1))
 {
  Chip_EVRT_ClrPendIntSrc(EVRT_SRC_BOD1);
 }
}

My Problem is, after I activate the IRQ NVIC_EnableIRQ(EVENTROUTER_IRQn);, the MCU jumps into the IRQ-handlder. Why?

Another Problem is, that I can not reset the Status reg via  Chip_EVRT_ClrPendIntSrc(EVRT_SRC_BOD1);  The function call has no effect?

What is wrong? Thank's for any Feedback!

1 解答
2,704 次查看
timokunze
Contributor I

Thanks for the reply. I resolved the problem. The problem was, that the IRQ was permanently active. You can Close this issue.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,705 次查看
timokunze
Contributor I

Thanks for the reply. I resolved the problem. The problem was, that the IRQ was permanently active. You can Close this issue.

0 项奖励
回复
2,704 次查看
jakeweiner
Contributor I

Having the exact same problems, can't seem to reset my event status (hence it gets stuck in the IRQ handler). Have you tried 

LPC_EVRT->CLR_STAT &= (0x01UL<<EVRT_SRC_BOD1); // clears the status register

If that doesnt work the only way I can actually get out of the IRQ is by doing


LPC_EVRT->CLR_EN = (0x01UL<<EVRT_SRC_BOD1); // disable the bod event bit in the enable register

But the 2nd command is pretty useless as you wouldn't use it in a real life application. 

Let me know if you've found a solution to the problem.

0 项奖励
回复