AudioOutputDevice works in keil examples but give distorted sound in lpcexpresso examples

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AudioOutputDevice works in keil examples but give distorted sound in lpcexpresso examples

1,677 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lundburgerr on Fri Apr 12 08:28:21 MST 2013

Compiling and running the usb audioOutputDevice example works great both on keil and on red suite 5 (using lpcexpresso examples), with one exception.


On red suite 5 the sound gets distorted in some way and I cannot find out why. I also noticed that I cannot get DEBUGOUT function to work in the lpcexpresso examples either but it works on the keil examples. (e.g the i2s example)


Is this a bug or am I missing something obvious, does it work fine for anyone else?
And also is it correct that the only differences between the keil examples and the lpcexpresso examples are the startup-files?


 


To be specific I am using the keil mcb1857 board.


Thanks in advance //Robin

Labels (1)
0 Kudos
Reply
2 Replies

1,659 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lundburgerr on Thu Apr 25 02:46:49 MST 2013

Thanks for your reply and sorry for my late reply, didn't go to work last week.
Setting USB_FORCED_FULLSPEED to 1 in the LPCUSBlibConfig.h file fixed issue with the distorted sound in the audioOutput device example.


As for the other issues, they seemed to resolve themselves with a fresh build not sure what I did so that they wouldn't work.
Thanks alot for your help!


//Robin 

0 Kudos
Reply

1,659 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tuong on Mon Apr 15 01:04:00 MST 2013

Hi,


 


Did you set USB_FORCED_FULLSPEED to 1? This example can only run in full speed.


About the DEBUGOUT, please make sure you called Board_Debug_Init(), this set UART3 as debug printing port, before calling DEBUGOUT("").


If those above checks do not give expected result, then please do a fresh build! This example must run out of box as I observed!


 


With best regards,

0 Kudos
Reply