Attach some flexcomm peripherals to core 1 with gcc sdk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Attach some flexcomm peripherals to core 1 with gcc sdk

2,276件の閲覧回数
train_hugo
Contributor I

Hi,

We are using LPC55S69-evk with the latest GCC based SDK (using CMake). We can't find out why for some peripherals, there is no suitable .cmake file for core 1 in the SDK. 

As an example, there is only a "component_flexcomm_i2c_adapter_LPC55S69_cm33_core0.cmake" but no "component_flexcomm_i2c_adapter_LPC55S69_cm33_core1.cmake. However according to the MCU's datasheet, it seems possible to map i2c to core 1...

Is there any particular reason for that ?

Best regards

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,259件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello train_hugo,

Sorry there is only SDK demo and compile for IDE version, no command version.

 

 

BR

Alice

0 件の賞賛
返信

2,237件の閲覧回数
train_hugo
Contributor I

Hi Alice,

I believe my question wasn't clear..

I'm not searching for any sdk demo, but I'm just trying to figure out why in the GCC sdk there seems not to be full support of peripherals such as i2c or spi or any other peripheral excepting the one listed in the screenshot below.

screen_gcc_sdk.jpgscreen_gcc_sdk.jpg

Should I write my own .cmake files for the missing peripherals for core1 or did I miss something ?

Best regards,

Hugo

0 件の賞賛
返信

2,229件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello train_hugo,

There isn't , you need write by yourself.

And almost project with LPC55s69 are based on IDE.

 

BR

Alice

0 件の賞賛
返信

2,224件の閲覧回数
frank_m
Senior Contributor III

> There isn't , you need write by yourself.

Not that it's very helpful, but ...

This is very common for free toolchains and SDKs. It is simply not possible or economic to provide support for every possible MCU/toolchain/example combination.

I have some experience with those from other providers.

 

0 件の賞賛
返信