Arduino board with the Dual CAN-FD Shield Board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Arduino board with the Dual CAN-FD Shield Board

2,356 次查看
bshannon1
Contributor II

I noticed that the OM13099 Dual CAN-FD Shield has similar pin outs to an Arduino board and can fit on top of it. Is it possible to code an Arduino board to send CAN/CAN-FD messages using the CAN-FD shield?

标记 (2)
0 项奖励
回复
2 回复数

2,056 次查看
soledad
NXP Employee
NXP Employee

Hi,

Yes, you can use the CAN-FD Shield, however, this is not supported by NXP.

 

Have a great day,

Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,056 次查看
bshannon1
Contributor II

Thank you for your response soledad. I understand that it is possible that the CAN Shield requires to use the SPI bus of the microcontroller and that this may not be supported by NXP. Do you know of any other references or methods for this to work? I'm just curious. 

0 项奖励
回复