Arduino board with the Dual CAN-FD Shield Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Arduino board with the Dual CAN-FD Shield Board

2,330件の閲覧回数
bshannon1
Contributor II

I noticed that the OM13099 Dual CAN-FD Shield has similar pin outs to an Arduino board and can fit on top of it. Is it possible to code an Arduino board to send CAN/CAN-FD messages using the CAN-FD shield?

タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,030件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Yes, you can use the CAN-FD Shield, however, this is not supported by NXP.

 

Have a great day,

Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,030件の閲覧回数
bshannon1
Contributor II

Thank you for your response soledad. I understand that it is possible that the CAN Shield requires to use the SPI bus of the microcontroller and that this may not be supported by NXP. Do you know of any other references or methods for this to work? I'm just curious. 

0 件の賞賛
返信