Alternate for LPC1769 for 12bit ADC Application

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Alternate for LPC1769 for 12bit ADC Application

1,479 次查看
TEMCEFF
Contributor IV

Dear All,
We have used LPC1769 for our application. We tried using LPC1769 for ADC application but it couldn't work and producing near full count for low analog input. We had gone through the Errata sheet and work around but we couldn't achieve the result. Kindly suggest us the Cortex-M based controller with 12bit at least 6 Channels ADC.

Application details : We want to scan all the 6 channels , single channel at a time in the time span of 2ms

Other requirements : UARTs :3, Timers :4 ,GPIOs 40,Flash : 256KB, RAM : 36KB

Also suggest us whether  LPC1519 suits for the above application

标签 (2)
标记 (1)
0 项奖励
回复
1 回复

1,291 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Anusha G,

Thank you for your interest in NXP Semiconductor products ans the opportunity to serve you.

According to your statement, I think the LPC1778FBD144 and LPC1519 both are good choice, and you can learn the more information about them through the link below.

http://www.nxp.com/documents/user_manual/UM10470.pdf 

http://www.nxp.com/documents/user_manual/UM10736.pdf
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复